REGEN.TESTTO

Description

This command is used to configure the timeout expected by the regen self-test feature. See REGEN.TEST for more info on how this timeout is used.

Versions

Action

Version

Notes

Implemented

02-07-03-000

General Information

Type

Read/Write

Units

Milliseconds

Range

1 to 4000

Default Value

1000

Data Type

Integer

See Also

REGEN.TEST
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
REGEN.TESTTO

3007h

09h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

REGEN.TESTTO

2408

968

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.TESTTO

2408

Unsigned16

Read/Write

-